debugger.SoftwareTraceLPD.Priority


This property sets or refers to the priority for the acquisition of software trace (LPD output) data. [RH850][E2]

[Specification format]

debugger.SoftwareTraceLPD.Priority = tracePriority

[Setting(s)]

Setting

Description

tracePriority

Set the priority for the acquisition of software trace (LPD output) data.

The values that can be specified are shown below.

Type

Description

TracePriority.SpeedPriority

Real-time operation is given priority in tracing.

TracePriority.DataPriority

The CPU pipeline is temporarily stopped so that no trace data is lost.

[Reference]

The current priority setting for the acquisition of software trace (LPD output) data

[Detailed description]

-

This property sets or refers to the current priority setting for the acquisition of software trace (LPD output) data.

[Example of use]

>>>print debugger.SoftwareTraceLPD.Priority
SpeedPriority
>>>debugger.SoftwareTraceLPD.Priority = TracePriority.DataPriority
>>>print debugger.SoftwareTraceLPD.Priority
DataPriority
>>>