This tab is used to set the build tool and debug tool plug-ins to be read in when this product is started.
Caution | We recommend that the check box for the plug-in for the microcontroller that is the target for development is not deselected.
Deselect the check boxes for the build tool and debug tool plug-ins that are for microcontrollers that are not the target for development. For example, if only the plug-in for the build tool is deselected, the file to be downloaded by the debug tool will not be found and an error will occur. |
Figure A.60 | Plug-in Manager Dialog Box: [Basic Function] Tab |
The following items are explained here.
[How to open]
- | From the [Tool] menu, select [Plug-in Setting...]. |
[Description of each area]
This area shows a list of the build tool and debug tool plug-ins installed in this product, in the following format.
|
Module Name
|
Shows the plug-in module names.
The plug-ins read in when this product is started are selected with check boxes.
|
|
Description
|
Shows a simple description of the plug-in.
|
[Function buttons]
|
|
|
|
OK
|
Applies all setting and closes this dialog box.
|
|
Cancel
|
Cancels the designated condition and closes the dialog box.
|
|
Help
|
Displays the help of this dialog box.
|