2.3.10 Indicating mismatches between versions registered with the license manager and the floating license server
The
balloon help that pops up from the
icon indicates mismatches between versions registered with the license manager and the floating license server.
Figure 2.17 | [Notification regarding the version of the license manager] Information Icon |
Figure 2.18 | [Notification regarding the version of the floating license server] Information Icon |
Clicking on the
icon or
balloon help will produce a message dialog box.