The following operations will enable you to customize the displaying of items (columns) and the analysis information on the Function List panel/Variable List panel.
All operations refer to the header area of each panel (the area where the column labels are displayed).
| In the Column Chooser dialog box, click the [Default] button to return all the customizations you have performed via the operations above to the default values. |