R_PICn_Timer_SyncStart


Generates start triggers of the timers for which simultaneous start is enabled.

[Syntax]

void    R_PICn_Timer_SyncStart ( void );

Remark

n is the unit number.

[Argument(s)]

None.

[Return value]

None.