Renesas Electronics
Below is a list of API functions output by the Code Generator for A/D converter use.
Table 3.19
API Functions: [A/D converter]
API Function Name
Function
R_ADCn_Create
Performs initialization necessary to control the A/D converter functions.
R_ADCn_Create_UserInit
Performs user-defined initialization relating to the A/D converter functions.
r_adcn_error_interrupt
Performs processing in response to the A/D error interrupt.
r_adcn_scan_groupm_end_interrupt
Performs processing in response to the scan group end interrupt.
r_adcn_multiplexer_request_interrupt
Performs processing in response to the MPX interrupt.
r_adcn_adc_summation_channelm_end_interrupt
Performs processing in response to the accumulation end interrupt.
R_ADCn_Halt
Halts A/D converter.
R_ADCn_SetMultiplexerCommand
Sets MPX command.
R_ADCn_ScanGroupm_Start
Starts ADC scan group conversion.
R_ADCn_ScanGroupm_GetResult
Reads the results of ADC scan group conversion.
R_ADCn_ScanGroupm_GetFloatingPointDataResult
Reads the results of ADC scan group conversion (converted to the floating-point format).
R_ADCn_ScanGroupm_TimerStart
Starts ADC scan group timer.
R_ADCn_ScanGroupm_TimerStop
Ends ADC scan group timer.
R_ADCn_ADCSummation_Cannelm_GetResult
Reads the results of accumulation data.
R_ADCn_ADCSummation_Start
Starts summation function.
R_ADCn_ADCSummation_Stop
Ends summation function.
R_ADC_SyncStart
Starts ADC scan group conversion set as enable scan group synchronization start.
R_ADC_SyncTimerStart
Starts ADC scan group conversion set as enable A/D timer synchronization start.
R_ADCn_ScanGroupm_OperationOn
Starts ADC scan group scan.
R_ADCn_TH_Groupx_Start
Starts ADC T&H group hold.
R_ADCn_TH_Sampling_Start
Starts ADC T&H sampling.