Starts CSI data transmission/reception.
Remark 1. This API function repeats the byte-level CSI transmission from the buffer specified in argument tx_buf the number of times specified in argument tx_num.
Remark 2. This API function performs byte-level CSI reception the number of times specified by the argument tx_num, and stores the data in the buffer specified by the argument rx_buf.
Remark 3. When performing a CSI reception, R_CSImn_Start must be called before this API function is called.
[Syntax]
#include r_cg_macrodriver.h
MD_STATUS
R_CSImn_Send_Receive ( uint8_t * const tx_buf, uint16_t
tx_num,
uint8_t * const rx_buf );
Remark m is the unit number, and n is the channel number.
[Argument(s)]
|
I/O |
Argument |
Description |
|
I |
uint8_t * const tx_buf; |
Pointer to a buffer storing the transmission data |
|
I |
uint16_t tx_num; |
Total amount of data to send/receive |
|
O |
uint8_t * const rx_buf; |
Pointer to a buffer to store the received data |
[Return value]
|
Macro |
Description |
|
MD_OK |
Normal completion |
|
MD_ARGERROR |
Invalid argument specification |