Below is a list of API functions output by the Code Generator for serial array unit use.
Table 3.30 API Functions: [Serial Array Unit] (1)
|
API Function Name |
Function |
|
Performs initialization necessary to control the serial array unit. | |
|
Performs user-defined initialization related to the serial array unit. | |
|
Reset the serial array unit. | |
|
Halts the clock supplied to the serial array unit. | |
|
Enables the switch from STOP mode to SNOOZE mode. | |
|
Disables the switch from STOP mode to SNOOZE mode. | |
|
Performs initialization necessary to perform the UART communication. | |
|
Performs processing in response to the UART transmission end interrupt INTSTn. | |
|
Performs processing in response to the UART reception end interrupt INTSRn. | |
|
Performs processing in response to the reception error interrupt INTSREn. | |
|
Sets UART communication to standby mode. | |
|
Ends UART communication. | |
|
Starts UART data transmission. | |
|
Starts UART data reception. | |
|
Performs processing in response to the UART transmission end interrupt INTSTn. | |
|
Performs processing in response to the UART reception end interrupt INTSRn. | |
|
Performs processing in response to the UART reception error interrupt INTSREn. | |
|
Performs processing in response to detection of overrun error. | |
|
Performs initialization necessary to perform the 3-wire serial I/O communication. | |
|
Performs processing in response to the CSI communication end interrupt INTCSImn. | |
|
Sets 3-wire serial I/O communication to standby mode. | |
|
Ends 3-wire serial I/O communication. | |
|
Starts CSI data transmission. | |
|
Starts CSI data reception. | |
|
Starts CSI data transmission/reception. | |
|
Performs processing in response to the CSI transmission end interrupt INTCSImn. |
Table 3.31 API Functions: [Serial Array Unit] (2)
|
API Function Name |
Function |
|
Performs processing in response to the CSI reception end interrupt INTCSImn. | |
|
Performs processing in response to the CSI reception error interrupt INTSREn. | |
|
Performs initialization necessary to perform the simplified IIC communication. | |
|
Performs processing in response to the simple IIC communication end interrupt INTIICmn. | |
|
Generates start conditions. | |
|
Generates stop conditions. | |
|
Ends simplified IIC communication. | |
|
Starts simple IIC master transmission. | |
|
Starts simple IIC master reception. | |
|
Performs processing in response to the simple IICmn master transmission end interrupt INTIICmn. | |
|
Performs processing in response to the simple IICmn master reception end interrupt INTIICmn. | |
|
Performs processing in response to detection of parity error (ACK error). |