r_elc_elsrni_interrupt

Performs processing in response to the event link interrupt.

Remark This API function is called to run interrupt processing for the event signal defined in event link setting register.
n is the source number.

[Syntax]

static void r_elc_elsrni_interrupt ( void );

Remark n is the source number.

[Argument(s)]

None.

[Return value]

None.