R_ELC_Set_PortBuffern

Sets the value of a port buffer.

[Syntax]

void R_ELC_Set_PortBuffern ( uint8_t value );

Remark n is the source number.

[Argument(s)]

I/O

Argument

Description

I

uint8_t value;

The value set in the port buffer.

[Return value]

None.