R_RTC_Set_BinaryAlarm

Sets the condition for the alarm interrupt (ALM) and allows detection of ALM (binary count mode).

[Syntax]

void R_RTC_Set_BinaryAlarm ( uint32_t alarm_enable, uint32_t alarm_val );

[Argument(s)]

I/O

Argument

Description

I

uint32_t alarm_enable;

Comparison flag

0x0 : Comparison does not proceed

0x1 : Comparison proceeds

I

uint32_t alarm_val;

The value of the binary counter

[Return value]

None.