R_RTC_Set_ConstPeriodInterruptOn

Sets the period of the periodic interrupt (PRD) and allows detection of the PRD.

[Syntax]

#include "r_cg_rtc.h"

void R_RTC_Set_ConstPeriodInterruptOn ( rtc_int_period_t period );

[Argument(s)]

I/O

Argument

Description

I

rtc_int_period_t period;

Period of the periodic interrupt (PRD).

PES_2_SEC : 2 seconds

PES_1_SEC : 1 second

PES_1_2_SEC : 1/2 second

PES_1_4_SEC : 1/4 second

PES_1_8_SEC : 1/8 second

PES_1_16_SEC : 1/16 second

PES_1_32_SEC : 1/32 second

PES_1_64_SEC : 1/64 second

PES_1_128_SEC : 1/128 second

PES_1_256_SEC : 1/256 second

[Return value]

None.