Performs user-defined initialization related to the FIFO embedded serial communications interface.
Remark This API function is called as the R_SCIFAn_Create callback routine.
[Syntax]
void R_SCIFAn_Create_UserInit ( void );
Remark n is the channel number.
[Argument(s)]
None.
[Return value]
None.