r_scifan_erif_interrupt

Performs processing in response to the framing error or parity error interrupts.

Remark This API function is called to run the interrupt processing for the framing error or parity error interrupt.

[Syntax]

static void r_scifan_erif_interrupt ( void );

Remark n is the channel number.

[Argument(s)]

None.

[Return value]

None.