APPENDIX A WINDOW REFERENCE
This appendix explains the window/panels that are used when the activation option for the CF850V4 is specified from the integrated development environment platform CS+.
This panel is used to display information regarding the node selected on the Project Tree panel and change the settings of the information.