tloc_mtx

Outline

Lock mutex (with timeout).

C format

 ER      tloc_mtx (ID mtxid, TMO tmout);
Parameter(s)

I/O

Parameter

Description

I

 ID      mtxid;
ID number of the mutex to be locked.

I

 TMO     tmout;
Specified timeout (unit:millisecond).

TMO_FEVR: Waiting forever.

TMO_POL: Polling.

Value: Specified timeout.



Explanation

This service call locks the mutex specified by parameter mtxid.

If the target mutex could not be locked (another task has been locked) when this service call is issued, this service call queues the invoking task to the target mutex wait queue and moves it from the RUNNING state to the WAITING state with timeout (mutex wait state).

The WAITING state for a mutex is cancelled in the following cases, and then moved to the READY state.

WAITING State for a Mutex Cancel Operation

Return Value

The locked state of the target mutex was cancelled as a result of issuing unl_mtx.

E_OK

The locked state of the target mutex was cancelled as a result of issuing ext_tsk.

E_OK

The locked state of the target mutex was cancelled as a result of issuing ter_tsk.

E_OK

Forced release from waiting (accept rel_wai while waiting).

E_RLWAI

Forced release from waiting (accept irel_wai while waiting).

E_RLWAI

Polling failure or timeout.

E_TMOUT



Note 1 Invoking tasks are queued to the target mutex wait queue in the order defined during configuration (FIFO order or priority order).

Note 2 In the RI850V4, E_ILUSE is returned if this service call is re-issued for the mutex that has been locked by the invoking task (multiple-locking of mutex).

Note 3 TMO_FEVR is specified for wait time tmout, processing equivalent to loc_mtx will be executed. When TMO_POL is specified, processing equivalent to ploc_mtx will be executed.

Return value

Macro

Value

Description

E_OK

0

Normal completion.

E_PAR

-17

Parameter error.

- tmout < TMO_FEVR

E_ID

-18

Invalid ID number.

- mtxid < 0x0

- mtxid > Maximum ID number

E_CTX

-25

Context error.

- This service call was issued from a non-task.

- This service call was issued in the CPU locked state.

- This service call was issued in the dispatching disabled state.

E_ILUSE

-28

Illegal service call use.

- Multiple locking of a mutex.

E_NOEXS

-42

Non-existent object.

- Specified mutex is not registered.

E_RLWAI

-49

Forced release from the WAITING state.

- Accept rel_wai/irel_wai while waiting.

E_TMOUT

-50

Timeout.

- Polling failure or timeout.