3.2.3 Error information

Error messages are output.

The output example of the error information is shown below.

*** Error Information ***
 
** E0562310 Undefined external symbol "_func_02" referenced in "sample.obj"     (1)

Number

Description

(1)

Error message

Error messages are output.