3.2.7 Contents of the Function List

If -show=cfi is specified, this option outputs the contents of the function list for use in detecting illegal indirect function calls.

The output example is given below.

*** CFI Table List ***
 
SYMBOL/ADDRESS
 
_func     (1)
0000F100  (2)

Number

Description

(1)

Outputs the symbol for the function.

(2)

Outputs the address of the function if a symbol for it has not been defined.