5.2.4  
Compiler output directives
 
Compiler output directives inform the assembler of information output by the compiler, such as compiler debugging information.
The following compiler output directives are available.
Table 5.11  | Compiler Output Directives  | 
 
| 
 | 
 | 
| 
 
.file 
 | 
 
Generates a symbol table entry 
 | 
| 
 
.line 
 | 
 
Line-number information from the C source program 
 | 
| 
 
.stack 
 | 
 
Defines the stack amount of consumption  for a symbol 
 | 
| 
 
._line_top 
 | 
 
Information specified by the compiler #pragma inline_asm statement 
 | 
| 
 
._line_end 
 | 
 
Information specified by the compiler #pragma inline_asm statement 
 |