Defines the stack size for a symbol.
[Syntax]
| 
 
Symbol field 
 | 
 
Mnemonic field 
 | 
 
Operand field 
 | 
 
Comment field 
 | 
  
 | 
.stack 
 | 
symble-name=value 
 | 
[; comment] 
 | 
 
[Function]
-  | Defines the stack size to be shown in Call Walker for a symbol.  | 
 
[Description]
-  | This defines the stack size to be shown in Call Walker for a symbol.  | 
 
-  | The stack size for a symbol can only be defined once, and subsequent definitions are ignored.  | 
 
-  | The stack size can only be defined as a 4-byte range of 0x0 to 0xFFFFFFFC.  If a different value is specified, then the definition is ignored.  | 
 
[Remark]
-  | See the user's manual of CS+ for details about Call Walker.  |