11.2 -Xcpu Option Specification for Assembler
The instructions that can be assembled differ depending on the parameter specified for the -Xcpu option. See the user's manual of the target device for the usable instructions. When an unusable instruction is written, an assemble error will occur and the following message will be output.
|
E0550269 : Illegal mnemonic(cannot use this mnemonic ins RH850 "core-name").
|