This dialog box is used to set an offset value of the start address in the address area on the Memory panel.
 
This section describes the following.
| On the Memory panel, select [View] >> [Address Offset Value Settings...] from the context menu. | 
Directly enter a hexadecimal value as an offset value for the address display.
The settable range depends on the number of bytes of the memory currently being displayed in a line on the Memory panel, as follows:
Settable range: 0x0 - ("Set value of [Size Notation]" x "The number of view columns") -1
| When "Set value of [Size Notation]" is 1 byte and "The number of view columns" is 16 columns: |