2.9.3 Display/change the SFR

Contents of the SFR can be displayed and its values can be changed in the SFR panel below.

Select the [View] menu >> [SFR].

For details on the contents and function in each area, see the section for the SFR panel.

Figure 2.105

Display the Contents of SFR (SFR Panel)

(1): [SFR] area

(2): [Value] area

(3): [Type (Byte Size)] area

(4): [Address] area

 

This section describes the following.

 

2.9.3.1 Search for a SFR

2.9.3.2 Organize SFRs

2.9.3.3 Change display format of values

2.9.3.5 Display/modify the SFR contents during program execution

2.9.3.5 Display/modify the SFR contents during program execution

2.9.3.6 Save the SFR contents