Renesas Electronics
Here, the points to note when you make settings of various events are described.
2.17.7.1 Allowable number of valid events
2.17.7.2 Types of events that can be set or removed during execution
2.17.7.3 Other precautions