2.17.7.3 Other precautions

-

No events can be set to local variables.

 

-

No events occur during step execution (including Return Out), as well as during program execution actuated by selecting [Go to Here] from the context menu.

 

-

If the program to be debugged is downloaded again and the position at which some existing event is set happens, as a consequence of it, to be in the middle of an instruction, the relevant event needs to be reset. Here is the method for doing it.

-

When debug information is available:
The event set position always moves to the beginning of source text lines.

-

When no debug information is available:
The position depends on how the [Automatic change method of event setting position] property in the [Download] category on the Property panel's [Download File Settings] tab is set.