2.14.3.2 Execute the program

Execute the program (see "2.9 Execute Programs").

When an instruction for which a timer start event or timer end event has been set is executed, a timer measurement is started or finished.

After execution of the program has stopped, the measurement result can be confirmed as a timer measurement event on the Events panel that is opened by choosing [Event] from the [View] menu, as shown below.

Note that this timer measurement event is a particular type of event that is displayed on only the Events panel when either a timer start event or a timer end event has been set.

Figure 2.162

Example of Measurement Results by Timer Measurement Event (Timer Start and End Events) [E1] [E20]

Figure 2.163 Example of Measurement Results by Timer Measurement Event (Timer Start and End Events)
[EZ Emulator]

Figure 2.164

Example of a Measurement Result by Timer Measurement Event (Timer Start and End Events) [Simulator]