2.2.1.2 [E20]

Connect a host machine and E20. If required, connect a target board, too.

You can make a choice between FINE communications [E20(Serial)] and JTAG communications [E20(JTAG)] as the communication method to the target system (see "2.3.1 Select the debug tool to use").

See E20 User's Manual for details on the connection method.

Figure 2.2

Connection Example [E20(JTAG)]

Figure 2.3

Connection Example [E20(Serial)]

Note

Use a 38-pin to 14-pin conversion adapter attached to the E20 emulator if you have selected FINE [E20 (Serial)] as the method of communication with the target system.
For more details on the connection using a 38-pin to 14-pin conversion adapter, see E20 User's Manual