2.11.3.3 Changing the form in which values are displayed

The form in which the data in the [Value] area is displayed can be freely changed using the toolbar buttons shown below.

Notation

Shows the following buttons that change the form in which values are displayed.

 

Hexadecimal

Displays the value of a selected item in hexadecimal (default).

Signed Decimal

Displays the value of a selected item in signed decimal.

Unsigned Decimal

Displays the value of a selected item in unsigned decimal.

Octal

Displays the value of a selected item in octal.

Binary

Displays the value of a selected item in binary.

ASCII

Displays the value of a selected item in ASCII code.

 

Adds a hexadecimal equivalent for the displayed value of a selected item at the end of the value, with the equivalent enclosed in parentheses ( ).