Property panel


This panel allows you to view the information on and change the setting for the node selected in the Project Tree panel.

Figure A.3

Property Panel

 

The following items are explained here.

[How to open]

-

On the Project Tree panel, select [Project name (Project)] >> [Pin Configurator (Design Tool)], and then select [Property] from the [View] menu.

-

On the Project Tree panel, select [Project name (Project)] >> [Pin Configurator (Design Tool)], and then select [Property] from the context menu.

-

On the Project Tree panel, select [Project name (Project)] >> [Pin Configurator (Design Tool)] >> [Device Pin List], and then select [Property] from the [View] menu.

-

On the Project Tree panel, select [Project name (Project)] >> [Pin Configurator (Design Tool)] >> [Device Pin List], and then select [Property] from the context menu.

-

On the Project Tree panel, select [Project name (Project)] >> [Pin Configurator (Design Tool)] >> [Device Top View], and then select [Property] from the [View] menu.

-

On the Project Tree panel, select [Project name (Project)] >> [Pin Configurator (Design Tool)] >> [Device Top View], and then select [Property] from the context menu.

Remark 1.

If this panel is already open, selecting a different [Pin Configurator (Design Tool)] in the Project Tree panel changes the content displayed accordingly.

Remark 2.

If this panel is already open, selecting a different [Device Pin List] in the Project Tree panel changes the content displayed accordingly.

Remark 3.

If this panel is already open, selecting a different [Device Top View] in the Project Tree panel changes the content displayed accordingly.

[Description of each area]

(1)

Detail information display/change area

This area allows you to view the information on and change the setting for the node selected in the Project Tree panel.

The content displayed in this area differs depending on the node selected in the Project Tree panel.

(2)

Tab selection area

In this panel, following tabs are contained (see the section explaining each tab for details on the display/setting on the tab).

[Context menu]

Undo

Cancels the effect of an edit operation to restore the previous state.

Cut

Sends the character string or lines selected with range selection to the clipboard and deletes them.

Copy

Sends the character string or lines selected with range selection to the clipboard.

Paste

Inserts the contents of the clipboard at the caret position.

Delete

Deletes the character string or the lines selected with the range selection.

Select All

Selects all strings displayed in the item being edited.