[Pin Configurator Settings] tab


This tab displays information (Product Information and Package) on the [Pin Configurator (Design Tool)] selected in the Project Tree panel.

Figure A.4

[Pin Configurator Settings] Tab

 

The following items are explained here.

[How to open]

-

On the Project Tree panel, select [Project name (Project)] >> [Pin Configurator (Design Tool)], and then select [Property] from the [View] menu.

-

On the Project Tree panel, select [Project name (Project)] >> [Pin Configurator (Design Tool)], and then select [Property] from the context menu.

Remark

If this panel is already open, selecting a different [Pin Configurator (Design Tool)] in the Project Tree panel changes the content displayed accordingly.

[Description of each area]

(1)

[Product Information] category

This area displays product information (Version and Release date) on Pin Configurator.

Version

Displays the version of Pin Configurator (Pin Configurator Plug-in).

Release date

Displays the release date of Pin Configurator (Pin Configurator Plug-in).

 

(2)

[Package] category

Change the shape (Package type) and settings of the microcontroller to display as the device top view in the Device Top View panel.

Package type

Selects the shape of the microcontroller displayed in the device top view.