Disconnecting a Debug Tool

When finishing debugging, disconnect the debug tool.

Click the Disconnect from Debug Tool button.

The status bar in the Main window shows [DISCONNECT] as shown below and the debugging finishes.

Tip

Downloading a program

If you change the program after downloading it to the target, you have to perform build process again and download the program. If you change the program after downloading, the right side of the line number turns yellow or green.