Running and Stopping the Program

Now that download of the load module file to the target is complete, you can run the program. First, run and stop the program.

1. Running the program

Run the program after resetting CPU.

Click the [Restart] button in the menu.

This runs the program and displays [RUN] in the status bar.

LEDs on RTK50565N2S10000BE light alternately.