Update Manager Options dialog box


This dialog box displays and changes the Update Manager options.

Figure A.10

Update Manager Options Dialog Box

 

The following items are explained here.

[How to open]

-

From the CS+ Update Manager window menu area, click [Change settings].

[Description of each area]

(1)

[Scheduled update check] area

(a)

[Category]

Select the category of for which to configure the behavior for found updates.

(b)

[If updates are found]

Set the behavior for found updates.

Select the action to perform for the selected category.

-

[Download updates automatically, and notify me when it’s finished.]

If corresponding updates are found during periodic checks for updates, download them without asking for confirmation, and notify the user when the download is complete.

-

[Notify me but do not automatically download them.]

If corresponding updates are found during periodic checks for updates, notify the user.

-

[Do nothing.]

If corresponding updates are found during periodic checks for updates, do not notify the user.

(2)

[Internet Connections] area

Describes the Internet connection.

[Function buttons]

Button

Function

OK

Finalizes the settings, reflects them, and closes the dialog box.

Cancel

Cancels any changes made to the settings, and closes the dialog box.