Renesas Electronics
top
with RI600V4
Analysis
FUNCTIONS
Open Analysis Result Panel
Limiting range of usage status
2.4.6 Limiting range of usage status
On the
Analysis Result panel
, by dragging and dropping with the mouse cursor in the
Execution transition display area
in the
Analysis information diagram area
, the user can change the analysis information to be displayed in the
Analysis information table area
from "analysis information in the trace data acquisition period" to "analysis information in the analysis information extraction interval".
It should be noted that the background for the
Analysis information extraction interval
that appears when the mouse cursor is dragged and dropped in the
Execution transition display area
assumes the magenta color.
Figure 2-8. Limiting Range of Usage Status
Remark By scrolling the
marks that are displayed directly below the
Start time of analysis information extraction
/
End time of analysis information extraction
, similar to the regular scroll bar, the user can change the
Analysis information extraction interval
.
Differences Information
Previous Topic
Zoom in or out of execution transition display
Next Topic
Clear Analysis Information
Table of Contents
On/Off of item display
Filtering of analysis information
Change of sort order
On/Off of display of state lines and event marks
Zoom in or out of execution transition display
Limiting range of usage status