Renesas Electronics
top
with RI600V4
Analysis
FUNCTIONS
Open Analysis Result Panel
2.4 Open Analysis Result Panel
To view analysis information, such as the state of processing program execution, the state of real-time OS resource usage, and the CPU usage status, open the
Analysis Result panel
.
The
Analysis Result panel
can be opened by pressing the
button which is located on the
Toolbar
on the
Realtime OS Task Analyzer panel
.
Figure 2-2. Analysis Result Panel
Remark The
Analysis Result panel
is displayed in the
Child-panel display area
on the
Realtime OS Task Analyzer panel
.
Differences Information
Previous Topic
Set Trace Start Event
Next Topic
On/Off of item display
Table of Contents
Overview
Open Realtime OS Task Analyzer Panel
Set Trace Start Event
Open Analysis Result Panel
On/Off of item display
Filtering of analysis information
Change of sort order
On/Off of display of state lines and event marks
Zoom in or out of execution transition display
Limiting range of usage status
Clear Analysis Information
Save Analysis Information
Restore Analysis Information