R_ATUIV_Timerknm_Get_CaptureValue


Reads the input capture register of the timer.

[Syntax]

void    R_ATUIV_Timerknm_Get_CaptureValue ( uint32_t * value );

Remark

k is the timer kind, n is the unit number, m is the channel number.

[Argument(s)]

I/O

Argument(s)

Description

O

uint32_t * value;

Pointer to area in which to store the results of input capture register

[Return value]

None.