R_ATUIV_Timerknm_Start_Down_Count


Starts the down count.

[Syntax]

void    R_ATUIV_Timerknm_Start_Down_Count ( void );

Remark

k is the timer kind, n is the unit number, m is the channel number.

[Argument(s)]

None.

[Return value]

None.