r_sci3m_callback_error


Performs processing in response to the SCI error interrupt.

Remark

This API function is called as the callback routine of interrupt process r_sci3m_interrupt_error corresponding to the SCI error interrupt.

[Syntax]

void    r_SCI3m_callback_error ( void );

Remark

m is the channel number.

[Argument(s)]

None.

[Return value]

None.