r_sci3m_callback_sendend


Performs processing in response to the SCI transmit interrupt.

Remark

This API function is called as the callback routine of interrupt process r_sci3m_interrupt_sendend corresponding to the SCI transmit interrupt.

[Syntax]

void    r_sci3m_callback_sendend ( void );

Remark

m is the channel number.

[Argument(s)]

None.

 

[Return value]

None.