Below is a list of API functions output by the Code Generator for Sampling output timer detector use.
Table 3.53 API Functions: [Sampling output timer detector]
|
API Function Name |
Funciton |
|
Performinitialization necessary to control the Sampling output timer detector. | |
|
Performs user-defined initialization relating to the Sampling output timer detector. | |
|
Performs processing in response to the Sampling output timer interval interrupt INTSMOTA. | |
|
performs processing in response to the Sampling output timer compare match interrupt INTSMOTB. | |
|
Performs processing int response to the Sampling detector detection interrupt INTSMPn. | |
|
Start Starts Sampling output timer detector. | |
|
Ends Sampling output timer detector. | |
|
Halts the clock supplied to the Sampling output timer detector. |