Below is a list of API functions output by the Code Generator for temperature sensor use.
Table 3.24 API Functions: [Temperature Sensor]
| API Function Name | Function | 
| Performs initialization necessary to control the temperature sensor. | |
| Performs user-defined initialization relating to the temperature sensor. | |
| Starts measurement of the temperature that uses the temperature sen sor. | |
| Ends measurement of the temperature that uses the temperature sensor. | |
| Reset the temperature sensor. | |
| Halts the clock supplied to the temperature sensor. |