r_cac_mendf_interrupt

Performs processing in response to the measurement end interrupt.

Remark This API function is called to run interrupt processing for the measurement end interrupt, which is generated when the clock frequency accuracy measurement circuit detects the valid edge of the reference signal.

[Syntax]

static void r_cac_mendf_interrupt ( void );

[Argument(s)]

None.

[Return value]

None.