Clock frequency accuracy measurement circuit (CAC)

Below is a list of API functions output by the Code Generator for clock frequency accuracy measurement circuit use.

Table 3.4 API Functions: [Clock Frequency Accuracy Measurement Circuit]

API Function Name

Function

R_CAC_Create

Performs initialization necessary to control the clock frequency accuracy measurement circuit.

R_CAC_Create_UserInit

Performs user-defined initialization relating to the clock frequency accuracy measurement circuit.

r_cac_mendf_interrupt

Performs processing in response to the measurement end interrupt.

r_cac_ferrf_interrupt

Performs processing in response to the frequency error interrupt.

r_cac_ovff_interrupt

Performs processing in response to the overflow interrupt.

R_CAC_Start

Starts measurement of the accuracy of the clock frequency.

R_CAC_Stop

Ends measurement of the accuracy of the clock frequency.