R_R12DAn_Set_ConversionValue

Sets the data for 12-bit D/A conversion.

[Syntax]

void R_R12DAn_Set_ConversionValue ( uint16_t reg_value );

Remark n is the channel number.

[Argument(s)]

I/O

Argument

Description

I

uint16_t reg_value;

Data for 12-bit D/A conversion

[Return value]

None.