12-bit D/A converter (R12DA)

Below is a list of API functions output by the Code Generator for 12-bit D/A converter use.

Table 3.32 API Functions: [12-Bit D/A Converter]

API Function Name

Function

R_R12DA_Create

Performs initialization necessary to control the 12-bit D/A converter.

R_R12DAn_Start

Starts D/A conversion.

R_R12DAn_Stop

Ends D/A conversion.

R_R12DAn_Set_ConversionValue

Sets the data for D/A conversion.

R_R12DA_Sync_Start

Starts synchronous D/A conversion.

R_R12DA_Sync_Stop

Ends synchronous D/A conversion.

R_R12DA_Create_UserInit

Performs user-defined initialization relating to the 12-bit D/A converter.