r_riicn_callback_receiveerror

Of the internal processing for transfer errors and event generation interrupts (EEI), this function handles processing specialized in the arbitration-lost detection, NACK detection, and timeout detection.

Remark This API function is called as the r_riicn_error_interrupt callback routine.

[Syntax]

#include "r_cg_macrodriver.h"

static void r_riicn_callback_receiveerror ( MD_STATUS status );

Remark n is the channel number.

[Argument(s)]

I/O

Argument

Description

I

MD_STATUS status;

Source of the transfer errors and event generation interrupts

MD_ERROR1 : Arbitration-lost detection

MD_ERROR2 : Timeout detection

MD_ERROR3 : NACK detection

[Return value]

None.