r_riicn_callback_transmitend

Of the internal processing for transfer errors and event generation interrupts (EEI), this function handles processing specialized in the start condition detection in response to calling of R_RIICn_Master_Send.

Remark This API function is called as the r_riicn_error_interrupt callback routine.

[Syntax]

static void r_riicn_callback_transmitend ( void );

Remark n is the channel number.

[Argument(s)]

None.

[Return value]

None.