[ RI600PX ] tab

Outline

This tab shows the detailed information on RI600PX to be used categorized by the following.

- Version Information

Display image





Explanation of each area

1 ) [Version Information]

The detailed information on the version of the RI600PX are displayed.

Kernel version

Display the version of RI600PX to be used.

Default

The version of the installed RI600PX

How to change

Changes not allowed

Install folder

Display the folder in which RI600PX to be used is installed with the absolute path.

Default

The folder in which RI600PX to be used is installed

How to change

Changes not allowed

Endian

Display the endian set in the project.

Display the same value as the value of the [Select endian] property of the build tool.

Default

The endian in the property of the build tool

How to change

Changes not allowed