del_alm

Outline

Delete alarm handler.

C format

 ER      del_alm (ID almid);
Parameter(s)

I/O

Parameter

Description

I

 ID      almid;
ID number of the alarm handler.



Explanation

This service call can be called from tasks that belong to Trusted Domain.

This service call deletes the alarm handler indicated by almid.

Return value

Macro

Value

Description

E_OK

0

Normal completion.

E_ID

-18

Invalid ID number.

- almid < 0

- almid > VTMAX_ALH

E_CTX

-25

Context error.

- This service call was issued in the CPU locked state.

- This service call was issued from non-task.

- This service call was issued in the status "PSW.IPL > kernel interrupt mask level".

E_MACV

-26

Memory access violation.

- Stack pointer points out of user stack for invoking task.

E_OACV

-27

Object access violation.

- The invoking task does not belong to trusted domain.

E_NOEXS

-42

Non-existent object.

- The alarm handler specified by almid does not exist.