del_cyc

Outline

Delete cyclic handler.

C format

 ER      del_cyc (ID cycid);
Parameter(s)

I/O

Parameter

Description

I

 ID      cycid;
ID number of the cyclic handler.



Explanation

This service call can be called from tasks that belong to Trusted Domain.

This service call deletes the cyclic handler indicated by cycid.

Return value

Macro

Value

Description

E_OK

0

Normal completion.

E_ID

-18

Invalid ID number.

- cycid < 0

- cycid > VTMAX_CYH

E_CTX

-25

Context error.

- This service call was issued in the CPU locked state.

- This service call was issued from non-task.

- This service call was issued in the status "PSW.IPL > kernel interrupt mask level".

E_MACV

-26

Memory access violation.

- Stack pointer points out of user stack for invoking task.

E_OACV

-27

Object access violation.

- The invoking task does not belong to trusted domain.

E_NOEXS

-42

Non-existent object.

- The cyclic handler specified by cycid does not exist.